AXIS#.PL.FB

Description

AXIS#.PL.FB returns the position feedback value. The value represents the feedback after the following operations have been performed:

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

N/A

Data Type

Float

See Also

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all variants.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.FB

6064h

00h

Signed32

Position

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5904

1

5904 (0x1710)

AXIS1.PL.FB

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PL.FB

5904

Signed32

Read Only

Position

Related Topics

"Position Loop"